MWDefineRegionsBuilderTranslucencyOptionType Enumeration

NXOpen.Tooling.MWDefineRegionsBuilder.TranslucencyOptionType is an alias for NXOpen.Tooling.MWDefineRegionsBuilderTranslucencyOptionType

class NXOpen.Tooling.MWDefineRegionsBuilderTranslucencyOptionType

Bases: object

This enum represents the translucency is to be performed on the selected or non-selected region faces

Enum Members

Enum Member Enum Member Description
SelectedFaces
Selected region faces
OtherFaces
Non-selected region faces
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.