MWCopySheetsBuilderTypes Enumeration

NXOpen.Tooling.MWCopySheetsBuilder.Types is an alias for NXOpen.Tooling.MWCopySheetsBuilderTypes

class NXOpen.Tooling.MWCopySheetsBuilderTypes

Bases: object

This enum represents the type of sheets to be copied

Enum Members

Enum Member Enum Member Description
PartingSurfaces
Sheet type - parting sheets
PatchedSurfaces
Sheet type - patched sheets
Both
Sheet type - Both parting and patched sheets
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.