LsdynaGeometryPreparationBuilderProcessType Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.ProcessType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderProcessType

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderProcessType

Bases: object

the enum of process type.

Enum Members

Enum Member Enum Member Description
Gravity
Blank has elastic deformation in flexible status.
Closing
The process of die travels from initial position to binder.
Drawing
The process of die travels from binder to punch.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.