LsdynaGeometryPreparationBuilderMaterialType Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.MaterialType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderMaterialType

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderMaterialType

Bases: object

the enum of material type.

Enum Members

Enum Member Enum Member Description
NXMaterial
Use NX material for LS-Dyna solver.
LSDynaMaterial
Use LS-Dyna material for LS-Dyna solver.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.