LsdynaGeometryPreparationBuilderDrawType Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.DrawType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderDrawType

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderDrawType

Bases: object

the enum of draw type.

Enum Members

Enum Member Enum Member Description
SingleDraw
For draw die, punch and binder are lower than die.
DoubleDraw
For draw die, punch and binder are higher than die.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.