LsdynaGeometryPreparationBuilderDrawBeadType Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.DrawBeadType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderDrawBeadType

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderDrawBeadType

Bases: object

the enum of draw bead type.

Enum Members

Enum Member Enum Member Description
Round
Draw bead section has round shape.
Rectangle
Draw bead section has rectangle shape.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.