LsdynaGeometryPreparationBuilderBlankPosition Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.BlankPosition is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderBlankPosition

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderBlankPosition

Bases: object

the enum of blank position.

Enum Members

Enum Member Enum Member Description
AboveBinder
Blank sheet body is above binder.
AboveBinderandPunch
Blank sheet body is above binder and punch.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.