LsdynaGeometryPreparationBuilderBlankOption Enumeration

NXOpen.Tooling.LsdynaGeometryPreparationBuilder.BlankOption is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderBlankOption

class NXOpen.Tooling.LsdynaGeometryPreparationBuilderBlankOption

Bases: object

the enum of blank option.

Enum Members

Enum Member Enum Member Description
Sheet
Select a sheet body as blank.
Curve
Select several curves to create a blank.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.