LsdynaFormAnalysisResultDisplayBuilderStressTypeName Enumeration

NXOpen.Tooling.LsdynaFormAnalysisResultDisplayBuilder.StressTypeName is an alias for NXOpen.Tooling.LsdynaFormAnalysisResultDisplayBuilderStressTypeName

class NXOpen.Tooling.LsdynaFormAnalysisResultDisplayBuilderStressTypeName

Bases: object

Options to set stress type to display for stress analysis result.

Enum Members

Enum Member Enum Member Description
MaximumInplaneStress
Display maximum in-plane stress.
MinimumInplaneStress
Display minimum in-plane stress.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.