LayoutRepositionBuilderType Enumeration

NXOpen.Tooling.LayoutRepositionBuilder.Type is an alias for NXOpen.Tooling.LayoutRepositionBuilderType

class NXOpen.Tooling.LayoutRepositionBuilderType

Bases: object

Represents the method of layout transform.

Enum Members

Enum Member Enum Member Description
Move
Move type
Copy
Copy type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.