LayoutRepositionBuilderMethod Enumeration

NXOpen.Tooling.LayoutRepositionBuilder.Method is an alias for NXOpen.Tooling.LayoutRepositionBuilderMethod

class NXOpen.Tooling.LayoutRepositionBuilderMethod

Bases: object

Represents the type of layout transform.

Enum Members

Enum Member Enum Member Description
Rotate
Rotate method
Transform
Transform method
PointToPoint
Point to Point method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.