LayoutBuilderLayoutType Enumeration

NXOpen.Tooling.LayoutBuilder.LayoutType is an alias for NXOpen.Tooling.LayoutBuilderLayoutType

class NXOpen.Tooling.LayoutBuilderLayoutType

Bases: object

Represents the type of layout.

Enum Members

Enum Member Enum Member Description
Rectangle
Rectangle layout
Circular
Circle layout
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.