LayoutBuilderLayoutSubType Enumeration

NXOpen.Tooling.LayoutBuilder.LayoutSubType is an alias for NXOpen.Tooling.LayoutBuilderLayoutSubType

class NXOpen.Tooling.LayoutBuilderLayoutSubType

Bases: object

Represents the the sub type of layout.

Enum Members

Enum Member Enum Member Description
Balance
Balance type
Linear
Linear type
Radial
Radial circular type
Constant
Constanct circular type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.