IntermediateStageCollection Class

class NXOpen.Tooling.IntermediateStageCollection

Bases: object

Creates a NXOpen.Tooling.IntermediateStageBuilder

To obtain an instance of this class, refer to NXOpen.Tooling.ToolingManager

New in version NX8.5.0.

Methods

Method Description
CreateIntermediateStageBuilder Creates create direct unfold builder @return
FindObject Finds the NXOpen.Tooling.IntermediateStageBuilder with the given identifier as recorded in a journal.

Method Detail

CreateIntermediateStageBuilder

IntermediateStageCollection.CreateIntermediateStageBuilder

Creates create direct unfold builder

Signature CreateIntermediateStageBuilder()

Returns:
Return type:NXOpen.Tooling.IntermediateStageBuilder

New in version NX8.5.0.

License requirements: None.

FindObject

IntermediateStageCollection.FindObject

Finds the NXOpen.Tooling.IntermediateStageBuilder with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier to be found
Returns:IntermediateStageBuilder found
Return type:NXOpen.Tooling.IntermediateStageBuilder

New in version NX8.5.0.

License requirements: None.