InsertAuxiliaryBuilderDesignToolOption Enumeration

NXOpen.Tooling.InsertAuxiliaryBuilder.DesignToolOption is an alias for NXOpen.Tooling.InsertAuxiliaryBuilderDesignToolOption

class NXOpen.Tooling.InsertAuxiliaryBuilderDesignToolOption

Bases: object

Specifies the design tool option.

Enum Members

Enum Member Enum Member Description
Copy
copy
Array
array
Delete
delete
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.