InsertAuxiliaryBuilderCircOperationTypes Enumeration

NXOpen.Tooling.InsertAuxiliaryBuilder.CircOperationTypes is an alias for NXOpen.Tooling.InsertAuxiliaryBuilderCircOperationTypes

class NXOpen.Tooling.InsertAuxiliaryBuilderCircOperationTypes

Bases: object

Specifies the options of circular array.

Enum Members

Enum Member Enum Member Description
Create
create
Edit
edit
Delete
delete
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.