InitProjBuilderProjTempOption Enumeration¶
NXOpen.Tooling.InitProjBuilder.ProjTempOption is an alias for NXOpen.Tooling.InitProjBuilderProjTempOption
-
class
NXOpen.Tooling.
InitProjBuilderProjTempOption
¶ Bases:
object
Represents the project template option of InitProj, defines the pre-defined project template.
this template will be used as the basic assembly structure for this new project
Enum Members
Enum Member Enum Member Description Default Indicates that the project template is ‘Default’. The members of enum are changed in opening dialog-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-