HoleReportBuilderTypes Enumeration¶
NXOpen.Tooling.HoleReportBuilder.Types is an alias for NXOpen.Tooling.HoleReportBuilderTypes
-
class
NXOpen.Tooling.
HoleReportBuilderTypes
¶ Bases:
object
Specifies the option of hole table type
Enum Members
Enum Member Enum Member Description CreateTable the hole table type of create hole tableUpdateTable the hole table type of update hole table-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-