HoleReportBuilderEnumSelectionType Enumeration

NXOpen.Tooling.HoleReportBuilder.EnumSelectionType is an alias for NXOpen.Tooling.HoleReportBuilderEnumSelectionType

class NXOpen.Tooling.HoleReportBuilderEnumSelectionType

Bases: object

Specifies the option of selection type to create hole table

Enum Members

Enum Member Enum Member Description
ViewSelection
Selects view to create hole table
WindowSelection
Selects holes in window to create hole table
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.