HoleReportBuilderEnumQuadrantType Enumeration

NXOpen.Tooling.HoleReportBuilder.EnumQuadrantType is an alias for NXOpen.Tooling.HoleReportBuilderEnumQuadrantType

class NXOpen.Tooling.HoleReportBuilderEnumQuadrantType

Bases: object

Specifies the option of which quadrant is positive

Enum Members

Enum Member Enum Member Description
PositiveQuadrantI
First quadrant is positive
PositiveQuadrantIi
Second quadrant is positive
PositiveQuadrantIii
Third quadrant is positive
PositiveQuadrantIv
Forth quadrant is positive
PositiveQuadrantAll
All quadrant is positive
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.