FormingInsertBuilderBlankPositions Enumeration

NXOpen.Tooling.FormingInsertBuilder.BlankPositions is an alias for NXOpen.Tooling.FormingInsertBuilderBlankPositions

class NXOpen.Tooling.FormingInsertBuilderBlankPositions

Bases: object

Specifies the blank position.

Enum Members

Enum Member Enum Member Description
PunchPlate
the blank is on the punch plate
StripperPlate
the blank is on the stripper plate
DiePlate
the blank is on the die plate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.