ForceCalculationBuilderProcessTypes Enumeration¶
NXOpen.Tooling.ForceCalculationBuilder.ProcessTypes is an alias for NXOpen.Tooling.ForceCalculationBuilderProcessTypes
-
class
NXOpen.Tooling.
ForceCalculationBuilderProcessTypes
¶ Bases:
object
The process type.
Enum Members
Enum Member Enum Member Description Catalog catalogAngularBlanking angular blankingAngularEmbossing angular embossingAngularPiercing angular piercingBending bendingBlanking blankingBurring burringCircularDrawing circular drawingCounterboring counterboringCountersinking countersinkingCylindricalIroning cylindrical ironingFlanging flangingPiercing piercingRoundEmbossing round embossingSquareDrawing square drawingUBending U bendingVBending V bendingVBendingTree V bending treeZBending Z bending-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-