ForceCalculationBuilderCalculationTypes Enumeration

NXOpen.Tooling.ForceCalculationBuilder.CalculationTypes is an alias for NXOpen.Tooling.ForceCalculationBuilderCalculationTypes

class NXOpen.Tooling.ForceCalculationBuilderCalculationTypes

Bases: object

The calculation type.

Enum Members

Enum Member Enum Member Description
Normal
calculate force considering pre-stations effects
Isolated
calculate force in isolation, without considering other processes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.