FastenerAssyStackTypeMethod Enumeration

NXOpen.Tooling.FastenerAssy.StackTypeMethod is an alias for NXOpen.Tooling.FastenerAssyStackTypeMethod

class NXOpen.Tooling.FastenerAssyStackTypeMethod

Bases: object

Represents screw_array type

Enum Members

Enum Member Enum Member Description
Screw
Screw type
TopStack
Top stack type
BottomStack
Bottom stack type
RootNode
Root node type
TopNode
Top node type
BottomNode
Bottom node type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.