FastenerAssySelectionTypeMethod Enumeration

NXOpen.Tooling.FastenerAssy.SelectionTypeMethod is an alias for NXOpen.Tooling.FastenerAssySelectionTypeMethod

class NXOpen.Tooling.FastenerAssySelectionTypeMethod

Bases: object

Represents selection type for position and hole

Enum Members

Enum Member Enum Member Description
Hole
Hole type
Position
Position type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.