FastenerAssySelectionObjectMethod Enumeration

NXOpen.Tooling.FastenerAssy.SelectionObjectMethod is an alias for NXOpen.Tooling.FastenerAssySelectionObjectMethod

class NXOpen.Tooling.FastenerAssySelectionObjectMethod

Bases: object

Represents selection object type

Enum Members

Enum Member Enum Member Description
Top
Top object
Bottom
Bottom object
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.