FastenerAssyHoleOperation Enumeration

NXOpen.Tooling.FastenerAssy.HoleOperation is an alias for NXOpen.Tooling.FastenerAssyHoleOperation

class NXOpen.Tooling.FastenerAssyHoleOperation

Bases: object

Represents the action on the hole menu of the fastener assembly.

Enum Members

Enum Member Enum Member Description
Add
Click the add hole group menu
Remove
Click the remove menu
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.