FaceSplitBuilderFaceSplitType Enumeration

NXOpen.Tooling.FaceSplitBuilder.FaceSplitType is an alias for NXOpen.Tooling.FaceSplitBuilderFaceSplitType

class NXOpen.Tooling.FaceSplitBuilderFaceSplitType

Bases: object

the type for Split Face

Enum Members

Enum Member Enum Member Description
CurvesEdges
using curve or edge for Split Face
Plane
using plane for Split Face
Intersection
using intersection curve of two body for Split Face
Isocline
using Isocline for Split Face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.