EnlargeSurfaceBuilder Class¶
-
class
NXOpen.Tooling.
EnlargeSurfaceBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges, curves, datum planes or faces.
Optionally creates output trimmed sheet body as a patch surface. To create a new instance of this class, use
NXOpen.Tooling.EnlargeSurfaceCollection.CreateEnlargeSurfaceBuilder()
Default values.
Property Value AsPatchSurface 1 ChangeAllSizes 1 CutToBoundary 1 RegionOption Keep SurfaceRange.AnchorPosition Vertex1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AsPatchSurface | Returns or sets the value of option, which specifies whether to set the result region as patch surface or not. |
BodyColor | Returns or sets the color value of patch surface body. |
BoundarySelection | Returns the selection of boundary to trim the target surface, it could be face, datum plane, edge and curve. |
ChangeAllSizes | Returns or sets the value of option, which specifies when enlarging surface, whether to change all the sizes at the same time or not. |
CutToBoundary | Returns or sets the value of option, which specifies whether to cut the target to boundary objects or not. |
DragData | Returns or sets the drag preview body data from builder according to face. |
RegionOption | Returns or sets the value of the option, which specifies to keep or discard the selected region. |
RegionSelection | Returns the selection of region, which will be kept or discarded as the result of enlarged surface. |
ReselTargetData | Returns or sets the reselect target face data from builder. |
SurfaceRange | Returns the surface range data, which controls the enlarged parameters of surface. |
Tag | Returns the Tag for this object. |
TargetSelection | Returns the selection of target to create enlarge surface, body face only. |
Methods¶
Method | Description |
---|---|
AddPlanarFaceData | Initializes the planar face data with face, and adds the data to builder. |
AddSurfaceData | Initializes the surface data with face, and adds the data to builder. |
Commit | Commits any edits that have been applied to the builder. |
CreatePreviewSurface | Create preview surface data from builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ErasePlanarFaceData | Erases the planar face data from builder according to face. |
EraseSurfaceData | Erases the surface data from builder according to face. |
GetColorValue | Returns the value of patch surface color. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetColorValue | Sets the value of patch surface color. |
SetRangeValue | Sets the value of surface range to buider data according to range face. |
SetTargetFace | Sets the target face to target surface data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EnlargeSurfaceBuilderKeepDiscardOption Enumeration | represents the keep discard options for selected region. |
Property Detail¶
AsPatchSurface¶
-
EnlargeSurfaceBuilder.
AsPatchSurface
¶ Returns or sets the value of option, which specifies whether to set the result region as patch surface or not.
-------------------------------------
Getter Method
Signature
AsPatchSurface()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AsPatchSurface(asPatchSurface)
Parameters: asPatchSurface (bool) – New in version NX7.5.0.
License requirements: None.
BodyColor¶
-
EnlargeSurfaceBuilder.
BodyColor
¶ Returns or sets the color value of patch surface body.
-------------------------------------
Getter Method
Signature
BodyColor()
Returns: the color index Return type: Id New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyColor(patchColor)
Parameters: patchColor (Id) – the color index New in version NX8.0.1.
License requirements: None.
BoundarySelection¶
-
EnlargeSurfaceBuilder.
BoundarySelection
¶ Returns the selection of boundary to trim the target surface, it could be face, datum plane, edge and curve.
-------------------------------------
Getter Method
Signature
BoundarySelection()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
ChangeAllSizes¶
-
EnlargeSurfaceBuilder.
ChangeAllSizes
¶ Returns or sets the value of option, which specifies when enlarging surface, whether to change all the sizes at the same time or not.
-------------------------------------
Getter Method
Signature
ChangeAllSizes()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChangeAllSizes(changeAllSizes)
Parameters: changeAllSizes (bool) – New in version NX7.5.0.
License requirements: None.
CutToBoundary¶
-
EnlargeSurfaceBuilder.
CutToBoundary
¶ Returns or sets the value of option, which specifies whether to cut the target to boundary objects or not.
-------------------------------------
Getter Method
Signature
CutToBoundary()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutToBoundary(cutToBoundary)
Parameters: cutToBoundary (bool) – New in version NX7.5.0.
License requirements: None.
DragData¶
-
EnlargeSurfaceBuilder.
DragData
¶ Returns or sets the drag preview body data from builder according to face.
-------------------------------------
Getter Method
Signature
DragData()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DragData(setDragData)
Parameters: setDragData (bool) – New in version NX8.5.0.
License requirements: None.
RegionOption¶
-
EnlargeSurfaceBuilder.
RegionOption
¶ Returns or sets the value of the option, which specifies to keep or discard the selected region.
-------------------------------------
Getter Method
Signature
RegionOption()
Returns: Return type: NXOpen.Tooling.EnlargeSurfaceBuilderKeepDiscardOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionOption(regionOption)
Parameters: regionOption ( NXOpen.Tooling.EnlargeSurfaceBuilderKeepDiscardOption
) –New in version NX7.5.0.
License requirements: None.
RegionSelection¶
-
EnlargeSurfaceBuilder.
RegionSelection
¶ Returns the selection of region, which will be kept or discarded as the result of enlarged surface.
-------------------------------------
Getter Method
Signature
RegionSelection()
Returns: Return type: NXOpen.RegionPointList
New in version NX7.5.0.
License requirements: None.
ReselTargetData¶
-
EnlargeSurfaceBuilder.
ReselTargetData
¶ Returns or sets the reselect target face data from builder.
-------------------------------------
Getter Method
Signature
ReselTargetData()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReselTargetData(setReselTargetData)
Parameters: setReselTargetData (bool) – New in version NX8.5.0.
License requirements: None.
SurfaceRange¶
-
EnlargeSurfaceBuilder.
SurfaceRange
¶ Returns the surface range data, which controls the enlarged parameters of surface.
-------------------------------------
Getter Method
Signature
SurfaceRange()
Returns: Return type: NXOpen.GeometricUtilities.SurfaceRangeBuilder
New in version NX7.5.0.
License requirements: None.
TargetSelection¶
-
EnlargeSurfaceBuilder.
TargetSelection
¶ Returns the selection of target to create enlarge surface, body face only.
-------------------------------------
Getter Method
Signature
TargetSelection()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
Method Detail¶
AddPlanarFaceData¶
-
EnlargeSurfaceBuilder.
AddPlanarFaceData
¶ Initializes the planar face data with face, and adds the data to builder.
Signature
AddPlanarFaceData(planarFace)
Parameters: planarFace ( NXOpen.Face
) – face to add to planar face dataNew in version NX7.5.0.
License requirements: None.
AddSurfaceData¶
-
EnlargeSurfaceBuilder.
AddSurfaceData
¶ Initializes the surface data with face, and adds the data to builder.
Signature
AddSurfaceData(addFace)
Parameters: addFace ( NXOpen.Face
) – face to add to surface dataNew in version NX7.5.0.
License requirements: None.
CreatePreviewSurface¶
-
EnlargeSurfaceBuilder.
CreatePreviewSurface
¶ Create preview surface data from builder.
Signature
CreatePreviewSurface()
New in version NX8.5.0.
License requirements: None.
ErasePlanarFaceData¶
-
EnlargeSurfaceBuilder.
ErasePlanarFaceData
¶ Erases the planar face data from builder according to face.
Signature
ErasePlanarFaceData(planarFace)
Parameters: planarFace ( NXOpen.Face
) – face to get planar face dataNew in version NX7.5.0.
License requirements: None.
EraseSurfaceData¶
-
EnlargeSurfaceBuilder.
EraseSurfaceData
¶ Erases the surface data from builder according to face.
Signature
EraseSurfaceData(eraseFace)
Parameters: eraseFace ( NXOpen.Face
) – face to get surface dataNew in version NX7.5.0.
License requirements: None.
GetColorValue¶
-
EnlargeSurfaceBuilder.
GetColorValue
¶ Returns the value of patch surface color.
Signature
GetColorValue()
Returns: a tuple Return type: A tuple consisting of (redValue, greenValue, blueValue). redValue is a float. red value between 0 and 1 greenValue is a float. green value between 0 and 1 blueValue is a float. blue value between 0 and 1 New in version NX7.5.0.
License requirements: None.
SetColorValue¶
-
EnlargeSurfaceBuilder.
SetColorValue
¶ Sets the value of patch surface color.
Signature
SetColorValue(redValue, greenValue, blueValue)
Parameters: - redValue (float) – red value between 0 and 1
- greenValue (float) – green value between 0 and 1
- blueValue (float) – blue value between 0 and 1
New in version NX7.5.0.
License requirements: None.
SetRangeValue¶
-
EnlargeSurfaceBuilder.
SetRangeValue
¶ Sets the value of surface range to buider data according to range face.
Signature
SetRangeValue(rangeFace, rangeValue)
Parameters: - rangeFace (
NXOpen.Face
) – range face - rangeValue (list of float) – array of u and v range value
New in version NX7.5.0.
License requirements: None.
- rangeFace (
SetTargetFace¶
-
EnlargeSurfaceBuilder.
SetTargetFace
¶ Sets the target face to target surface data.
Signature
SetTargetFace(targetFace)
Parameters: targetFace ( NXOpen.Face
) – target faceNew in version NX7.5.0.
License requirements: None.
Validate¶
-
EnlargeSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.