ElectrodeCopyBuilderCopy Enumeration

NXOpen.Tooling.ElectrodeCopyBuilder.Copy is an alias for NXOpen.Tooling.ElectrodeCopyBuilderCopy

class NXOpen.Tooling.ElectrodeCopyBuilderCopy

Bases: object

Represents an index to copy type

Enum Members

Enum Member Enum Member Description
Transform
the method is transform
Mirror
the method is mirror
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.