ElectrodeComponentBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeComponentBuilder
¶ Bases:
NXOpen.Builder
Electrode component builder to install holder and pallet.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateComponentBuilder()
Default values.
Property Value ReferPart 0 Rename 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ChuckType | Returns or sets the electrode chuck type. |
Face | Returns the face whose center will be the origin of the machine set csys. |
Fixture | Returns the part which is an electrode fixture to be edited. |
MateCsys | Returns or sets the current machine set CSYS. |
Parent | Returns the part which is the assembly parent to install an electrode chuck. |
ReferPart | Returns or sets the option to install a chuck by referring to the template part directly or not. |
Rename | Returns or sets the option to use the part name management dialog box or not. |
StandardData | Returns or sets the electrode standard data spraedsheet. |
StandardPart | Returns or sets the electrode standard part to be installed. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElectrodeComponentBuilderChuck Enumeration | Represents the electrode chuck type. |
Property Detail¶
ChuckType¶
-
ElectrodeComponentBuilder.
ChuckType
¶ Returns or sets the electrode chuck type.
-------------------------------------
Getter Method
Signature
ChuckType()
Returns: Return type: NXOpen.Tooling.ElectrodeComponentBuilderChuck
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChuckType(chuck)
Parameters: chuck ( NXOpen.Tooling.ElectrodeComponentBuilderChuck
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Face¶
-
ElectrodeComponentBuilder.
Face
¶ Returns the face whose center will be the origin of the machine set csys.
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectFace
New in version NX8.0.0.
License requirements: None.
Fixture¶
-
ElectrodeComponentBuilder.
Fixture
¶ Returns the part which is an electrode fixture to be edited.
-------------------------------------
Getter Method
Signature
Fixture()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
MateCsys¶
-
ElectrodeComponentBuilder.
MateCsys
¶ Returns or sets the current machine set CSYS.
-------------------------------------
Getter Method
Signature
MateCsys()
Returns: Return type: NXOpen.NXObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MateCsys(csys)
Parameters: csys ( NXOpen.NXObject
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Parent¶
-
ElectrodeComponentBuilder.
Parent
¶ Returns the part which is the assembly parent to install an electrode chuck.
-------------------------------------
Getter Method
Signature
Parent()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
ReferPart¶
-
ElectrodeComponentBuilder.
ReferPart
¶ Returns or sets the option to install a chuck by referring to the template part directly or not.
-------------------------------------
Getter Method
Signature
ReferPart()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferPart(referPart)
Parameters: referPart (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Rename¶
-
ElectrodeComponentBuilder.
Rename
¶ Returns or sets the option to use the part name management dialog box or not.
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
StandardData¶
-
ElectrodeComponentBuilder.
StandardData
¶ Returns or sets the electrode standard data spraedsheet.
-------------------------------------
Getter Method
Signature
StandardData()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardData(standardData)
Parameters: standardData (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
StandardPart¶
-
ElectrodeComponentBuilder.
StandardPart
¶ Returns or sets the electrode standard part to be installed.
-------------------------------------
Getter Method
Signature
StandardPart()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardPart(standardPart)
Parameters: standardPart (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Method Detail¶
Validate¶
-
ElectrodeComponentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.