EjectorPostProcessingBuilderTrimMethod Enumeration

NXOpen.Tooling.EjectorPostProcessingBuilder.TrimMethod is an alias for NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod

class NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod

Bases: object

The processing type: Trim, Adjust length and Untrim.

Enum Members

Enum Member Enum Member Description
AdjustLength
Adjust Length
SheetTrim
Sheet Trim
Untrim
Untrim
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.