EdgePatchBuilderSelectTypes Enumeration

NXOpen.Tooling.EdgePatchBuilder.SelectTypes is an alias for NXOpen.Tooling.EdgePatchBuilderSelectTypes

class NXOpen.Tooling.EdgePatchBuilderSelectTypes

Bases: object

Settings of the selection types.

Enum Members

Enum Member Enum Member Description
Face
Face types
Body
Body types
Traverse
Traverse types
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.