EdgePatchBuilderPatchStatus Enumeration

NXOpen.Tooling.EdgePatchBuilder.PatchStatus is an alias for NXOpen.Tooling.EdgePatchBuilderPatchStatus

class NXOpen.Tooling.EdgePatchBuilderPatchStatus

Bases: object

Settings of the patch status types.

Enum Members

Enum Member Enum Member Description
NoLoopExisted
No loop existed in list
OneLoopExisted
One loop existed in list
MultiLoopsExisted
More than one loops existed in list
SomeLoopsExisted
Some loops existed in list
LoopNotPatched
No loop is patched
PatchedAndSomeSuppressed
Some patched bodies are suppressed
PatchedAndAllSuppressed
All patched bodies are suppressed
PatchedAndNoSuppressed
No patched body is suppressed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.