DirectUnfoldBuilderTypes Enumeration

NXOpen.Tooling.DirectUnfoldBuilder.Types is an alias for NXOpen.Tooling.DirectUnfoldBuilderTypes

class NXOpen.Tooling.DirectUnfoldBuilderTypes

Bases: object

Specifies the option of direct unfold type

Enum Members

Enum Member Enum Member Description
Convert
the direct unfold type of convert to Sheet Metal
MergeBends
the direct unfold type of merge bends
DefinePreBends
the direct unfold type of define pre-bends
DeleteBends
the direct unfold type of delete all bends
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.