DirectUnfoldBuilderMatType Enumeration

NXOpen.Tooling.DirectUnfoldBuilder.MatType is an alias for NXOpen.Tooling.DirectUnfoldBuilderMatType

class NXOpen.Tooling.DirectUnfoldBuilderMatType

Bases: object

The material database defined in PDW.

It is added in project initialization.

Enum Members

Enum Member Enum Member Description
Steel
Default is steel.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.