DirectUnfoldBuilderBend Enumeration

NXOpen.Tooling.DirectUnfoldBuilder.Bend is an alias for NXOpen.Tooling.DirectUnfoldBuilderBend

class NXOpen.Tooling.DirectUnfoldBuilderBend

Bases: object

The number of children bends in defining prebend.

Enum Members

Enum Member Enum Member Description
Two
two bends
Three
three bends
Four
four bends
Five
five bends
Six
six bends
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.