DieInsertBuilderInsertModeItems Enumeration¶
NXOpen.Tooling.DieInsertBuilder.InsertModeItems is an alias for NXOpen.Tooling.DieInsertBuilderInsertModeItems
-
class
NXOpen.Tooling.
DieInsertBuilderInsertModeItems
¶ Bases:
object
Specifies the insert mode for die.
Enum Members
Enum Member Enum Member Description StandardInsert The die insert mode is standard insertSketchProfile The die insert mode is sketch profileBoundingBox The die insert mode is bounding box-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-