DieEngStampingOutputBuilder Class¶
-
class
NXOpen.Tooling.
DieEngStampingOutputBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Stamping Output builder
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieEngStampingOutputBuilder()
Default values.
Property Value SewTolerance 0.0254 SpringbackMethod None New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SewTolerance | Returns or sets the sew tolerance |
SourceBody | Returns the select die engineering sheet bodies |
SpringbackMethod | Returns or sets the springback method |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns the select target body |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
DefineSpringback | The define springback method |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProperty | The set stamping output display property method |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DieEngStampingOutputBuilderDisplayProductType Enumeration | Types of product display. |
DieEngStampingOutputBuilderSpringbackMethodType Enumeration | Types of springback method |
Property Detail¶
SewTolerance¶
-
DieEngStampingOutputBuilder.
SewTolerance
¶ Returns or sets the sew tolerance
-------------------------------------
Getter Method
Signature
SewTolerance()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SewTolerance(sewTolerance)
Parameters: sewTolerance (float) – New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SourceBody¶
-
DieEngStampingOutputBuilder.
SourceBody
¶ Returns the select die engineering sheet bodies
-------------------------------------
Getter Method
Signature
SourceBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SpringbackMethod¶
-
DieEngStampingOutputBuilder.
SpringbackMethod
¶ Returns or sets the springback method
-------------------------------------
Getter Method
Signature
SpringbackMethod()
Returns: Return type: NXOpen.Tooling.DieEngStampingOutputBuilderSpringbackMethodType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpringbackMethod(springbackMethod)
Parameters: springbackMethod ( NXOpen.Tooling.DieEngStampingOutputBuilderSpringbackMethodType
) –New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TargetBody¶
-
DieEngStampingOutputBuilder.
TargetBody
¶ Returns the select target body
-------------------------------------
Getter Method
Signature
TargetBody()
Returns: Return type: NXOpen.SelectBody
New in version NX10.0.0.
License requirements: None.
Method Detail¶
DefineSpringback¶
-
DieEngStampingOutputBuilder.
DefineSpringback
¶ The define springback method
Signature
DefineSpringback()
New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetProperty¶
-
DieEngStampingOutputBuilder.
SetProperty
¶ The set stamping output display property method
Signature
SetProperty()
New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Validate¶
-
DieEngStampingOutputBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.