DieEngLineupBuilder Class¶
-
class
NXOpen.Tooling.
DieEngLineupBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Die Engineer lineup management builder.
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieEngLineUpBuilder()
Default values.
Property Value ReorientProperties 0 UpdatePressInformation 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Product | Returns the lineup product sheet body |
ReorientProperties | Returns or sets the reorient properties |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UpdatePressInformation | Returns or sets the update press information |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
MoreDetails | The more details button call back |
ObjectProperties | The object properties button call back |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Product¶
-
DieEngLineupBuilder.
Product
¶ Returns the lineup product sheet body
-------------------------------------
Getter Method
Signature
Product()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ReorientProperties¶
-
DieEngLineupBuilder.
ReorientProperties
¶ Returns or sets the reorient properties
-------------------------------------
Getter Method
Signature
ReorientProperties()
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
ReorientProperties(reorientProperties)
Parameters: reorientProperties (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
UpdatePressInformation¶
-
DieEngLineupBuilder.
UpdatePressInformation
¶ Returns or sets the update press information
-------------------------------------
Getter Method
Signature
UpdatePressInformation()
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
UpdatePressInformation(updatePressInformation)
Parameters: updatePressInformation (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
MoreDetails¶
-
DieEngLineupBuilder.
MoreDetails
¶ The more details button call back
Signature
MoreDetails()
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ObjectProperties¶
-
DieEngLineupBuilder.
ObjectProperties
¶ The object properties button call back
Signature
ObjectProperties()
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Validate¶
-
DieEngLineupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.