DieBaseBuilderTypes Enumeration

NXOpen.Tooling.DieBaseBuilder.Types is an alias for NXOpen.Tooling.DieBaseBuilderTypes

class NXOpen.Tooling.DieBaseBuilderTypes

Bases: object

die base types.

Enum Members

Enum Member Enum Member Description
StandardDieBase
standard die base
CustomizeDieBase
customize die base
DesignTools
die base design tools
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.