DieBaseBuilderPlatesNumberOpt Enumeration

NXOpen.Tooling.DieBaseBuilder.PlatesNumberOpt is an alias for NXOpen.Tooling.DieBaseBuilderPlatesNumberOpt

class NXOpen.Tooling.DieBaseBuilderPlatesNumberOpt

Bases: object

plates number options.

Enum Members

Enum Member Enum Member Description
PlateFive
plates number is 5
PlateEight
plates number is 8
PlateNine
plates number is 9
PlateTen
plates number is 10
PlateTwelve
plates number is 12
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.