DieBaseBuilderParentNodeOpt Enumeration¶
NXOpen.Tooling.DieBaseBuilder.ParentNodeOpt is an alias for NXOpen.Tooling.DieBaseBuilderParentNodeOpt
-
class
NXOpen.Tooling.
DieBaseBuilderParentNodeOpt
¶ Bases:
object
parent node options.
Enum Members
Enum Member Enum Member Description Control use PDW project’s control part as parent partDie use PDW project’s die part as parent partSubFirst use PDW project’s sub-die base as parent partSubSecond use PDW project’s sub-die base as parent partDieBaseFirst use PDW project’s die base part as parent part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-