DieBaseBuilderDesignToolOption Enumeration¶
NXOpen.Tooling.DieBaseBuilder.DesignToolOption is an alias for NXOpen.Tooling.DieBaseBuilderDesignToolOption
-
class
NXOpen.Tooling.
DieBaseBuilderDesignToolOption
¶ Bases:
object
design tool options.
Enum Members
Enum Member Enum Member Description Split split sub die baseMerge merge sub die baseAlign align sub die baseAdjust adjust length of sub die baseSave save sub die base as templateDelete delete selected die base-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-