DefineLifterBuilderTypes Enumeration

NXOpen.Tooling.DefineLifterBuilder.Types is an alias for NXOpen.Tooling.DefineLifterBuilderTypes

class NXOpen.Tooling.DefineLifterBuilderTypes

Bases: object

Specifies the lifter types

Enum Members

Enum Member Enum Member Description
GenericLifter
Generic lifter type
LifteronLifter
Lifter on lifter type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.