CreateBoxBuilder Class¶
-
class
NXOpen.Tooling.
CreateBoxBuilder
¶ Bases:
NXOpen.Builder
Represents a box creation operation
To create a new instance of this class, use
NXOpen.Tooling.CreateBoxCollection.CreateBoxBuilder()
Default values.
Property Value Clearance.Value 1.0 (millimeters part), 0.1 (inches part) OffsetNegativeX.Value 1.0 (millimeters part), 0.1 (inches part) OffsetNegativeY.Value 1.0 (millimeters part), 0.1 (inches part) OffsetNegativeZ.Value 1.0 (millimeters part), 0.1 (inches part) OffsetPositiveX.Value 1.0 (millimeters part), 0.1 (inches part) OffsetPositiveY.Value 1.0 (millimeters part), 0.1 (inches part) OffsetPositiveZ.Value 1.0 (millimeters part), 0.1 (inches part) XValue.Value 10 (millimeters part), 1.0 (inches part) YValue.Value 10 (millimeters part), 1.0 (inches part) ZValue.Value 10 (millimeters part), 1.0 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BoxColor | Returns or sets the box color. |
Clearance | Returns the clearance value for box in six directions. |
Objects | Returns the objects used for bounding box creation. |
OffsetNegativeX | Returns the offset value for box in -X direction. |
OffsetNegativeY | Returns the offset value for box in -Y direction. |
OffsetNegativeZ | Returns the offset value for box in -Z direction. |
OffsetPositiveX | Returns the offset value for box in +X direction. |
OffsetPositiveY | Returns the offset value for box in +Y direction. |
OffsetPositiveZ | Returns the offset value for box in +Z direction. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the box type. |
XValue | Returns the edge length in X direction for general box. |
YValue | Returns the edge length in Y direction for general box. |
ZValue | Returns the edge length in Z direction for general box. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
ConvertFrecToBuilderData | Convert feature record data to builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBoxCsysPosition | Gets point position of csys for box. |
GetBoxFeatTag | Gets kf box feature tag. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetBoxColorValue | Sets box color. |
SetBoxCsysPosition | Sets point position of csys for box. |
SetBoxMatrixAndPosition | Sets box csys matrix. |
SetSelectedOccs | Sets selected object occurrences. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CreateBoxBuilderBoxType Enumeration | the type for creating box |
Property Detail¶
BoxColor¶
-
CreateBoxBuilder.
BoxColor
¶ Returns or sets the box color.
-------------------------------------
Getter Method
Signature
BoxColor()
Returns: Return type: int New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
BoxColor(colorValue)
Parameters: colorValue (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
Clearance¶
-
CreateBoxBuilder.
Clearance
¶ Returns the clearance value for box in six directions.
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Objects¶
-
CreateBoxBuilder.
Objects
¶ Returns the objects used for bounding box creation.
-------------------------------------
Getter Method
Signature
Objects()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeX¶
-
CreateBoxBuilder.
OffsetNegativeX
¶ Returns the offset value for box in -X direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeX()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeY¶
-
CreateBoxBuilder.
OffsetNegativeY
¶ Returns the offset value for box in -Y direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeY()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeZ¶
-
CreateBoxBuilder.
OffsetNegativeZ
¶ Returns the offset value for box in -Z direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeZ()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveX¶
-
CreateBoxBuilder.
OffsetPositiveX
¶ Returns the offset value for box in +X direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveX()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveY¶
-
CreateBoxBuilder.
OffsetPositiveY
¶ Returns the offset value for box in +Y direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveY()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveZ¶
-
CreateBoxBuilder.
OffsetPositiveZ
¶ Returns the offset value for box in +Z direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveZ()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Type¶
-
CreateBoxBuilder.
Type
¶ Returns or sets the box type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.CreateBoxBuilderBoxType
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.CreateBoxBuilderBoxType
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
XValue¶
-
CreateBoxBuilder.
XValue
¶ Returns the edge length in X direction for general box.
-------------------------------------
Getter Method
Signature
XValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
YValue¶
-
CreateBoxBuilder.
YValue
¶ Returns the edge length in Y direction for general box.
-------------------------------------
Getter Method
Signature
YValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ZValue¶
-
CreateBoxBuilder.
ZValue
¶ Returns the edge length in Z direction for general box.
-------------------------------------
Getter Method
Signature
ZValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
ConvertFrecToBuilderData¶
-
CreateBoxBuilder.
ConvertFrecToBuilderData
¶ Convert feature record data to builder.
Signature
ConvertFrecToBuilderData(featTag)
Parameters: featTag ( NXOpen.NXObject
) – bounding box kf feature tagNew in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
GetBoxCsysPosition¶
-
CreateBoxBuilder.
GetBoxCsysPosition
¶ Gets point position of csys for box.
Signature
GetBoxCsysPosition()
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GetBoxFeatTag¶
-
CreateBoxBuilder.
GetBoxFeatTag
¶ Gets kf box feature tag.
Signature
GetBoxFeatTag()
Returns: bounding box kf feature Return type: NXOpen.NXObject
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetBoxColorValue¶
-
CreateBoxBuilder.
SetBoxColorValue
¶ Sets box color.
Signature
SetBoxColorValue(value)
Parameters: value ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
SetBoxCsysPosition¶
-
CreateBoxBuilder.
SetBoxCsysPosition
¶ Sets point position of csys for box.
Signature
SetBoxCsysPosition(value)
Parameters: value ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
SetBoxMatrixAndPosition¶
-
CreateBoxBuilder.
SetBoxMatrixAndPosition
¶ Sets box csys matrix.
Signature
SetBoxMatrixAndPosition(matrix, position)
Parameters: - matrix (
NXOpen.Matrix3x3
) – - position (
NXOpen.Point3d
) –
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
- matrix (
SetSelectedOccs¶
-
CreateBoxBuilder.
SetSelectedOccs
¶ Sets selected object occurrences.
Signature
SetSelectedOccs(selections, deselections)
Parameters: - selections (list of
NXOpen.NXObject
) – Last selected objects. - deselections (list of
NXOpen.NXObject
) – Last deselected objects.
New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”) OR studio_free_form (“STUDIO FREE FORM”) OR features_modeling (“FEATURES MODELING”) OR solid_modeling (“SOLIDS MODELING”)
- selections (list of
Validate¶
-
CreateBoxBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.