CornerDesignBuilderTypes Enumeration

NXOpen.Tooling.CornerDesignBuilder.Types is an alias for NXOpen.Tooling.CornerDesignBuilderTypes

class NXOpen.Tooling.CornerDesignBuilderTypes

Bases: object

The corner design type.

Enum Members

Enum Member Enum Member Description
Create
Create operation
Edit
Edit operation
Delete
Delete operation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.