CornerDesignBuilderCornerTypeOpt Enumeration

NXOpen.Tooling.CornerDesignBuilder.CornerTypeOpt is an alias for NXOpen.Tooling.CornerDesignBuilderCornerTypeOpt

class NXOpen.Tooling.CornerDesignBuilderCornerTypeOpt

Bases: object

the corner types

Enum Members

Enum Member Enum Member Description
Chamfer
chamfer
Fillet
fillet
Mickey
mickey
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.