CompDrawingBuilderProjectionType Enumeration

NXOpen.Tooling.CompDrawingBuilder.ProjectionType is an alias for NXOpen.Tooling.CompDrawingBuilderProjectionType

class NXOpen.Tooling.CompDrawingBuilderProjectionType

Bases: object

Specifies the project type.

Enum Members

Enum Member Enum Member Description
FirstAngleProjection
first angle projection
ThirdAngleProjection
third angle projection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.