CompDrawingBuilderComponentTypeSelection Enumeration

NXOpen.Tooling.CompDrawingBuilder.ComponentTypeSelection is an alias for NXOpen.Tooling.CompDrawingBuilderComponentTypeSelection

class NXOpen.Tooling.CompDrawingBuilderComponentTypeSelection

Bases: object

Specifies the type of components.

Enum Members

Enum Member Enum Member Description
All
the type of components, read from configuration file
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.